Standard Injection Port Sampling
Revolutionary Sampling Tools along with Traditional Methodology
Vapor headspace sampling and introduction for GC/MS
The Headspace Sampling accessory provides the ability to prepare water or soil samples and then inject them into the Griffin GC/MS for analysis. Users can place up to six vials containing water or soil samples into the vial tray. The sampler then heats the vials, which sends any Volatile Organic Compounds (VOCs) into the vapor headspace. Using the syringe holder, the user manually draws an air sample from the headspace into the gas tight syringe and then injects the air sample into the GC injector. The Griffin GC/MS analyzes the sample according to previously determined method parameters and performs full identification of any VOCs found in the sample.