Fido® XT Explosives Detector
Portable, Handheld Explosives Detection
Fieldable, Trace Explosives Detection
Due to its small footprint and true vapor detection capabilities, the Fido Portable Explosives Detector is well suited to both handheld and robot-mounted applications. The tethered sensor head on the Fido XT provides incredible maneuverability while also allowing the sensor to be detached and integrated as a payload on numerous unmanned systems.
People Screening
The Fido Explosives Detectors are sensitive enough to detect the trace residue of explosives materials on a person and their effects that results from the construction or deployment of an explosive device. The speed and accuracy with which the Fido can detect such minute quantities makes it suitable for use at checkpoints or random searches.
Vehicle Screening
During the transportation or deployment of an explosive device, a vehicle will become contaminated with trace amounts of explosive residue in numerous areas. In some instances, such contamination can be so pervasive that detection can occur even when the explosive device is out of direct sight. The incredible sensitivity of the Fido Explosives Detector allows this contamination to be sampled and detected, providing useful evidence and intelligence even when a terrorist is not caught in the act.
IED Detection
Originally developed for humanitarian demining operations, the Fido is capable of detecting the vapor emanating from an improvised explosive device. The small size allows it to be integrated onto a robotic platform for remote detection operations. Though the Fido is capable of detecting the explosive device itself, by using it during checkpoint and people screening operations the Fido can also aid in the capture of the bomb-maker preventing the bomb from ever being emplaced.
Forensics Screening
The sensitivity and portability of the Fido Explosives Detector, combined with its onboard memory make it eminently suitable to forensic applications. Responders can take samples from the exterior of a vehicle or facility suspected to house bomb-making paraphernalia or from the suspect himself. These quantitative explosives detection results can be saved and printed to help establish justifiable cause or to back up expert witness testimony.
Cargo Screening
Trace detection and high volume sampling techniques utilizing vapor detection as a method increase the ability to detect concealed explosives even when explosive particulates are not present. As an ultra-sensitive trace explosive vapor detector, the Fido can be effectively employed for cargo, mail and baggage screening operations.
To find out more about countering threats from explosives in real world applications, contact the Fido team at 405.372.9535 or email us at fido@icxt.com.