Radiation Glossary

ADC
abbreviation of:Analog-to-digital converter

An analog-to-digital converter (abbreviated ADC, A/D or A to D) is an electronic circuit that converts continuous signals to discrete digital numbers. The reverse operation is performed by a digital-to-analog converter (DAC). Typically, an ADC is an electronic device that converts an input analog voltage (or current) to a digital number. (Source: Wikipedia)

ANSI
acronym of:American National Standards Institute

The American National Standards Institute or ANSI is a private nonprofit organization that oversees the development of voluntary consensus standards for products, services, processes, systems, and personnel in the United States. ANSI accredits standards that are developed by representatives of standards developing organizations, government agencies, consumer groups, companies, and others. (Source: Wikipedia)

Bq
abbreviation of:Becquerel

The becquerel (symbol Bq) is the SI derived unit of radioactivity, defined as the activity of a quantity of radioactive material in which one nucleus decays per second. It is therefore equivalent to s-1. (Source: Wikipedia)

cps
abbreviation of:Counts per Second
Cs
abbreviation of:Caesium

Caesium is a chemical element in the periodic table that has the symbol Cs and atomic number 55. It is a soft silvery-gold alkali metal with a melting point of 28 °C (83 °F) which makes it one of the metals that are liquid at or near room temperature along with rubidium (39°C), francium (27 °C), mercury (-39 °C), and gallium (30 °C). (Source: Wikipedia)

DSP
abbreviation of:Digital Signal Processing

Digital signal processing (DSP) is the study of signals in a digital representation and the processing methods of these signals. DSP and analog signal processing are subfields of signal processing. Since the goal of DSP is usually to measure or filter continuous real-world analog signals, the first step is usually to convert the signal from an analog to a digital form, by using an analog to digital converter. Often, the required output signal is another analog output signal, which requires a digital to analog converter. (Source: Wikipedia)

GM
abbreviation of:Geiger-Mueller

A Geiger-Müller tube (or GM tube) is the sensing element of a Geiger counter instrument that can detect a single particle of ionizing radiation, and typically produce an audible click for each. It was named for Hans Geiger who invented the device in 1908, and Walther Müller who collaborated with Geiger in developing it further in 1928. It is a type of a gaseous ionization detector. (Source: Wikipedia)

He
abbreviation of:Helium

Helium (He) is a colorless, odorless, tasteless, non-toxic, nearly inert monatomic chemical element that heads the noble gas series in the periodic table and whose atomic number is 2. Its boiling and melting points are the lowest among the elements and it exists only as a gas except in extreme conditions. Extreme conditions are also needed to create the small handful of helium compounds, which are all unstable at standard temperature and pressure. (Source: Wikipedia)

HV
abbreviation of:High Voltage
ICMP
acronym of:Internet Control Message Protocol

The Internet Control Message Protocol (ICMP) is one of the core protocols of the Internet protocol suite. It is chiefly used by networked computers' operating systems to send error messages—indicating, for instance, that a requested service is not available or that a host or router could not be reached. (Source: Wikipedia)

IEEE
acronym of:Institute of Electrical and Electronics Engineers

The Institute of Electrical and Electronics Engineers or IEEE is an international non-profit, professional organization for the advancement of technology related to electricity. (Source: Wikipedia)

IPv6
acronym of:Internet Protocol version 6

Internet Protocol version 6 (IPv6) is a network layer protocol for packet-switched internetworks. It is designated as the successor of IPv4, the current version of the Internet Protocol, for general use on the Internet. (Source: Wikipedia)

LaBr
abbreviation of:Lanthan Bromid

Lanthanum bromide (LaBr3) is a bromide of lanthanum, an inorganic compound. It has the appearance of a white powder or hexagonal crystals with melting point 789 °C. It is highly hygroscopic and well-soluble. It is used as a source of lanthanum in chemical synthesis. (Source: Wikipedia)

LCD
acronym of:Liquid crystal display

A liquid crystal display (commonly abbreviated LCD) is a thin, flat display device made up of any number of color or monochrome pixels arrayed in front of a light source or reflector. It is prized by engineers because it uses very small amounts of electric power, and is therefore suitable for use in battery-powered electronic devices. (Source: Wikipedia)

LED
abbreviation of:Light Emitting Diode

A light-emitting diode (LED) is a semiconductor device that emits incoherent narrow-spectrum light when electrically biased in the forward direction. This effect is a form of electroluminescence.
(Source: Wikipedia)

LLD
abbreviation of:Lower level discriminator

The LLD discriminates the lowest level of signal acquisition. Which means the lowest voltage required for a signal to be registered is defined here. Like ULD
the set ups 0 – 255 are not directly related to the channels.

mAh
abbreviation of:milliampere-hour

An ampere-hour (abbreviated as Ah or A-h is a unit of electric charge. One ampere-hour is equal to 3600 coulombs (ampere-seconds), and is the amount of electric charge transferred by a steady current of one ampere for one hour. The commonly seen milliampere-hour (mAh) is equal to 3.6 coulombs. (Source: Wikipedia)

MCA
abbreviation of:Multi Channel Analyser

Pulse amplitude analyser sorting the pulses of energy-proportional detectors according to the amplitude and thus the radiation energy and recording them in the corresponding channel. Multi-channel analysers have more than 8,000 channels. (Source: European Nuclear Society)

MCS
abbreviation of:MULTICHANNEL SCALING

The acquisition of time-correlated data in an MCA. Each channel is sequentially allocated a dwell time (a specified time period) for accumulating counts until all the memory has been addressed. MCS is useful for studying rapidly decaying radioactive sources. (Source: Canberra)

NaI
abbreviation of:Sodium iodide

Sodium iodide is a white, crystalline salt with chemical formula Na I used in radiation dectection, treatment of iodine deficiency, and as a catalyst in the Finkelstein reaction.

NiCd
acronym of:Nickel-cadmium battery

The nickel-cadmium battery is a popular type of rechargeable battery for portable electronics and toys using the metals nickel (Ni) and cadmium (Cd) as the active chemicals. (Source: Wikipedia)

NIM
abbreviation of:Nuclear Instrument Module
NiMH
abbreviation of:Nickel metal hydride battery

A nickel metal hydride battery, abbreviated NiMH, is a type of rechargeable battery similar to a nickel-cadmium ( Ni Cd) battery but has a hydrogen-absorbing alloy for the anode instead of cadmium. Like in NiCd batteries, nickel is the cathode. (Source: Wikipedia)

NORM
acronym of:Naturally Occurring Radioactive Material
PCI
acronym of:Peripheral Component Interconnect

The Peripheral Component Interconnect, or PCI Standard (in practice almost always shortened to PCI) specifies a computer bus for attaching peripheral devices to a computer motherboard. (Source: Wikipedia)

PHA
abbreviation of:Pulse height analysis

In the case of proportional counters , scintillators  or solid state detectors we know that the pulses leaving the detector have amplitudes proportional to the energy which the particles or photons deposit in the detectors. If these pulses are sorted according to their height, this would be the equivalent to sorting the particles or photons according to their energy. Electronic systems which do this are available and are called pulse height analyzer , or PHA's. (Source: TRIUMF Radiation Protection Training Course)

PMT
abbreviation of:Photomultiplier

Photomultiplier tubes (photomultipliers or PMTs for short) are extremely sensitive detectors of light in the ultraviolet, visible and near infrared. These detectors multiply the signal produced by incident light by as much as 108, from which single photons can be resolved. The combination of high gain, low noise, high frequency response and large area of collection have meant that these devices still find applications in nuclear and particle physics, astronomy, medical imaging and motion picture film scanning ( telecine). (Source: Wikipedia)

PoE
abbreviation of:Power over Ethernet

Power over Ethernet or PoE technology describes a system to transmit electrical power, along with data, to remote devices over standard twisted-pair cable in an Ethernet network. This technology is useful for powering IP telephones, wireless LAN access points, webcams, Ethernet hubs, embedded computers, and other appliances where it would be inconvenient or infeasible to supply power separately. (Source: Wikipedia)

RIID
acronym of:Radio-Isotope Identification Devices
RISC
acronym of:Reduced instruction set computer

The reduced instruction set computer, or RISC, is a CPU design philosophy that favors a reduced instruction set as well as a simpler set of instructions. The most common RISC microprocessors are Alpha, ARC, ARM, AVR, MIPS, PA-RISC, PIC, Power Architecture, and SPARC. (Source: Wikipedia)

RJ45
acronym of:Registered jack

A registered jack (RJ) is a standardized physical interface for connecting telecommunications equipment (commonly, a telephone jack) or computer networking equipment. The standard designs for these connectors and their wiring are named RJ11, RJ14, RJ45, etc. (Source: Wikipedia)

ROI
abbreviation of:Region Of Interest
RS232
acronym of:Serial binary data interconnection

In telecommunications, RS-232 is a standard for serial binary data interconnection between a DTE ( Data terminal equipment) and a DCE ( Data Circuit-terminating Equipment). It is commonly used in computer serial ports. (Source: Wikipedia)

SNTP
acronym of:Simple Network Time Protocol

A less complex form of NTP that does not require storing information about previous communications is known as the Simple Network Time Protocol or SNTP. It is used in some embedded devices and in applications where high accuracy timing is not required. (Source: Wikipedia)

TCP
acronym of:Transmission Control Protocol

The Transmission Control Protocol (TCP) is one of the core protocols of the Internet protocol suite, often simply referred to as TCP/IP. Using TCP, applications on networked hosts can create connections to one another, over which they can exchange streams of data using Stream Sockets. The protocol guarantees reliable and in-order delivery of data from sender to receiver. (Source: Wikipedia)

Tl
abbreviation of:Thallium

Thallium is a chemical element in the periodic table that has the symbol Tl and atomic number 81. [1] This soft gray malleable poor metal resembles tin but discolors when exposed to air. (Source: Wikipedia)

UDP
acronym of:User Datagram Protocol

The User Datagram Protocol (UDP) is one of the core protocols of the Internet protocol suite. Using UDP, programs on networked computers can send short messages sometimes known as datagrams (using Datagram Sockets) to one another. UDP is sometimes called the Universal Datagram Protocol or Unreliable Datagram Protocol. (Source: Wikipedia)

ULD
abbreviation of:Upper level discriminator

ULD discriminates the upper level of the signal acquisition. The voltage, which may not be exceeded by the signal in order to be registered, is defined here. Please note that the settings 0 to 255 don't belong to a channel directly, but 0 relates to the lowest channel and 255 to the top channel.

USB
acronym of:Universal Serial Bus

Universal Serial Bus (USB) is a serial bus standard to interface devices. It was originally designed for personal computers, but it has become commonplace on handheld devices such as portable memory devices, video game consoles, PDAs and portable media players. (Source: Wikipedia)

X-ray
acronym of:Röntgen rays

X-rays (or Röntgen rays) are a form of electromagnetic radiation with a wavelength in the range of 10 to 0.01 nanometers, corresponding to frequencies in the range 30 to 30 000 PHz (1015 hertz). X-rays are primarily used for diagnostic radiography and crystallography. X-rays are a form of ionizing radiation and as such can be dangerous. (Source: Wikipedia)

XML
acronym of:Extensible Markup Language

The Extensible Markup Language (XML) is a W3C-recommended general-purpose markup language. The XML recommendation specifies both the structure of XML, and the requirements for XML processors. XML is considered "general-purpose" because it enables anyone to originate and use a markup language for many types of applications and problem domains. (Source: Wikipedia)