2008-07-23

ICx Technologies Adds Stride Radionuclide Identification Detection Units and Systems to its Sophisticated Roster of Detection Products

ICx TechnologiesTM (NASDAQ: ICXT), a developer of advanced sensor technologies for homeland security, force protection and commercial applications, announced today the release of StrideTM Radionuclide Detection and Identification Systems.

WASHINGTON (July 23, 2008) - ICx TechnologiesTM (NASDAQ: ICXT), a developer of advanced sensor technologies for homeland security, force protection and commercial applications, announced today the release of StrideTM Radionuclide Detection and Identification Systems. Stride Systems are designed to automatically screen people, luggage and packages at critical checkpoints, as well as entries into facilities, to detect the covert movement of special nuclear materials or weapons. These systems are fully automatic, can be linked to the facilities' current security network and do not require sophisticated interpretation of results.

Stride systems can effectively detect and deter one of the most significant security threats by recognizing the presence of radioactive materials in buildings, at large public gatherings or events, at ports, bus or train stations, inside luggage or freight, at stadium entrances or at any other location of potential risk. Depending on the amount of radioactive material present, radionuclides can be detected and properly identified in a few seconds while security personnel are alerted via visible or audible annunciators.

"Radiation remains one of our main threats, and the lack of protection for critical facilities and entry points today is troubling," said Juergen Stein, head of the ICx Radiation business unit. "Stride offers the first automated radiation-detection solution that allows security managers to integrate advanced radiation detectors into their existing infrastructure," he continued. "Stride has the reliable spectroscopic accuracy of the ICx identiFINDERTM," which is the world's radiation-technology leader," added Stein.

Stride comes in three versions. The Stride Series 200 detection units have been designed primarily for fixed-wired installations. They can be mounted on walls, above doorways, behind reception desks, behind passport control counters, and above luggage or parcel conveyer belts.

The Series 300 Stanchion detection product was designed primarily for pedestrian security installations. This instrument detects and identifies radioactive material and yet looks exactly the same as a standard, crowd-control stanchion.

The Series 800 Portal detection units are used to establish a pedestrian portal into secure facilities. They utilize two large detectors and can detect extremely small amounts of radiation and identify the isotope in as few as one to three seconds.

All Stride products can immediately categorize radiation as innocent, suspicious or threatening and further identify the radionuclide as medical, industrial, naturally occurring or special nuclear material. Detection units initiate alarms based on dose-rate changes that are above background. The units can be set up with either a wired or a wireless communication to a Local Area Network, and will send a remote alert to other PCs, PDAs and the like insuring a rapid and appropriate response.

About FLIR Systems

FLIR Systems, Inc. is a world leader in the design, manufacture, and marketing of sensor systems that enhance perception and awareness. The Company’s advanced thermal imaging and threat detection systems are used for a wide variety of imaging, thermography, and security applications, including airborne and ground-based surveillance, condition monitoring, research and development, manufacturing process control, search and rescue, drug interdiction, navigation, transportation safety, border and maritime patrol, environmental monitoring, and chemical, biological, radiological, nuclear, and explosives (CBRNE) detection. Visit the Company's web site at www.FLIR.com.

The statements in this release by Earl R. Lewis, and the other statements in this release about the award described above, are forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995. Such statements are based on current expectations, estimates and projections about the Company's business based, in part, on assumptions made by management. These statements are not guarantees of future performance and involve risks and uncertainties that are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in such forward-looking statements due to numerous factors, including the following: the ability to manufacture and deliver the systems referenced in this release, changes in demand for the Company's products, product mix, the timing of deliveries under the award discussed above, the impact of competitive products and pricing, constraints on supplies of critical components, excess or shortage of production capacity, the ability of the Company to manufacture and ship products in the time period required, actual purchases under agreements, the Company's continuing compliance with U.S. export control laws and regulations, the timely receipt of export licenses for international shipments, the continuing eligibility of the Company to act as a federal contractor, and other risks discussed from time to time in the Company's Securities and Exchange Commission filings and reports. In addition, such statements could be affected by general industry and market conditions and growth rates, and general domestic and international economic conditions. Such forward-looking statements speak only as of the date on which they are made and the Company does not undertake any obligation to update any forward-looking statement to reflect events or circumstances after the date of this release, or for changes made to this document by wire services or Internet service providers.

All trademarks, registered trademarks and service marks are the property of their respective owners.

Media Contacts

Angel Bennett
FLIR, Systems, Inc.

2800 Crystal Drive, Suite 330
Arlington, VA 22202
angel.bennett@flir.com