2008-11-18

ICx Technologies Introduces the radHUNTER™ Radiation Detector

Designed for applications requiring speed and accuracy

WASHINGTON (Nov. 18, 2008) — ICx Technologies (NASDAQ: ICXT), a developer of advanced sensor technologies for homeland security, force protection and commercial applications, announced today the release of the radHUNTER™, an extremely sensitive and accurate digital, hand-held, gamma radionuclide identification device (RIID).

The radHUNTER is the culmination of more than eight years of development work on miniature, digital-signal processing electronics, utilizing operating-power conservation and advancements in the scintillation detector and the radionuclide template matching identification algorithm. Development of the radHUNTER was supported in part by the U.S. Department of Homeland Security (DHS)/Domestic Nuclear Detection Office (DNDO), as part of the Human Portable Radiation Detection System (HPRDS) procurement program.

Variations in normal operating conditions can affect the performance of RIIDs with scintillation detectors such as NaI and LaBr. Dramatic temperature variations can also affect the scintillation detector and/or the photo-multiplier tube (PMT), and can also cause instabilities and non-linearities in the electronics. In addition, high count-rates can impact the peak position in a spectrum. The radHUNTER’s instruments have been developed to correct all these circumstances through automatic calibration and continuous LED stabilization providing a high-performance instrument requiring little or no maintenance.

The radHUNTER is designed for first responders, customs agents, and specialized security forces. It was ergonomically constructed for easy operation with hazmat gloves; it has a simple, two-button operation for menu navigation, and starts up immediately in “find and identify” mode. It can label isotopes as NORM (Naturally Occurring Radioactive Material), industrial, medical or Special Nuclear Material, and has corresponding alarms that indicate the severity of the threat – all delivered in just seconds. For more information please visit www.icxt.com.

About FLIR Systems

FLIR Systems, Inc. is a world leader in the design, manufacture, and marketing of sensor systems that enhance perception and awareness. The Company’s advanced thermal imaging and threat detection systems are used for a wide variety of imaging, thermography, and security applications, including airborne and ground-based surveillance, condition monitoring, research and development, manufacturing process control, search and rescue, drug interdiction, navigation, transportation safety, border and maritime patrol, environmental monitoring, and chemical, biological, radiological, nuclear, and explosives (CBRNE) detection. Visit the Company's web site at www.FLIR.com.

The statements in this release by Earl R. Lewis, and the other statements in this release about the award described above, are forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995. Such statements are based on current expectations, estimates and projections about the Company's business based, in part, on assumptions made by management. These statements are not guarantees of future performance and involve risks and uncertainties that are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in such forward-looking statements due to numerous factors, including the following: the ability to manufacture and deliver the systems referenced in this release, changes in demand for the Company's products, product mix, the timing of deliveries under the award discussed above, the impact of competitive products and pricing, constraints on supplies of critical components, excess or shortage of production capacity, the ability of the Company to manufacture and ship products in the time period required, actual purchases under agreements, the Company's continuing compliance with U.S. export control laws and regulations, the timely receipt of export licenses for international shipments, the continuing eligibility of the Company to act as a federal contractor, and other risks discussed from time to time in the Company's Securities and Exchange Commission filings and reports. In addition, such statements could be affected by general industry and market conditions and growth rates, and general domestic and international economic conditions. Such forward-looking statements speak only as of the date on which they are made and the Company does not undertake any obligation to update any forward-looking statement to reflect events or circumstances after the date of this release, or for changes made to this document by wire services or Internet service providers.

All trademarks, registered trademarks and service marks are the property of their respective owners.

Media Contacts

Angel Bennett
FLIR, Systems, Inc.

2800 Crystal Drive, Suite 330
Arlington, VA 22202
angel.bennett@flir.com

LATEST VIDEOS


Star SAFIRE HD product video

Star SAFIRE® HD Family V2

identiFINDER product video

Introducing identiFINDER® 2