2008-01-22

ICx Releases Enzyme-Based Chemical Agent Detection Spray

Detects Nerve Agents with Fast, Reliable Pre- and Post-Decontamination Results

ICx™ Technologies (NASDAQ: ICXT), a developer of advanced technology solutions for homeland and military security, announced today the availability of ICx Agentase Disclosure Spray, an enzyme-based, chemical-agent-detection system in a spray formulation, which changes color when sprayed on surfaces contaminated with nerve agents.

Agentase Disclosure Spray pinpoints the exact location of agents on surfaces, allowing decontamination teams to accurately focus their regimens. Post-decontamination, the spray helps ensure that affected areas have been thoroughly cleaned.

"The use of chemical warfare agents (CWAs) is a significant terrorist threat, with multiple incidents occurring in Asia, Europe, and North America over the past 10 to 12 years," said Keith LeJeune, CEO, of ICx Agentase. "As a result, the ability to easily detect the presence of CWAs—both before and after decontamination of a site—is becoming a critical necessity of U.S. defense and civilian government agencies."

Agentase Disclosure Spray’s active ingredients are stored as powders for extended shelf-life, and are dissolved in water just prior to deployment through the use of a two-chamber sprayer. Color enhancers and thickeners enable usage on dark-colored surfaces or on areas with unusual geometries. The spray also carries components devised to illustrate when surfaces are too basic or too acidic for agent detection.

In the field, Agentase Disclosure Spray can detect the presence of CWAs at sub microgram levels within five minutes, eliminating the need for costly and time-consuming sampling, transportation, and laboratory analysis of potentially harmful agents. Time is of particular importance because of the risks of multiple exposures to, and possible re-transmissions of, nerve agents.

ICx developed the spray formulation in response to requests by current users of the ICx Agentase CAD-Kit™, a proven, highly selective detection system for nerve, blood, and blister agents that works without the need for training-intensive, power-dependent electronic instrumentation. The CAD-Kit, as well as Agentase Disclosure Spray, provide emergency responders and other critical personnel with simple, rapid, and reliable access to chemical-agent detection.

About FLIR Systems

FLIR Systems, Inc. is a world leader in the design, manufacture, and marketing of sensor systems that enhance perception and awareness. The Company’s advanced thermal imaging and threat detection systems are used for a wide variety of imaging, thermography, and security applications, including airborne and ground-based surveillance, condition monitoring, research and development, manufacturing process control, search and rescue, drug interdiction, navigation, transportation safety, border and maritime patrol, environmental monitoring, and chemical, biological, radiological, nuclear, and explosives (CBRNE) detection. Visit the Company's web site at www.FLIR.com.

The statements in this release by Earl R. Lewis, and the other statements in this release about the award described above, are forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995. Such statements are based on current expectations, estimates and projections about the Company's business based, in part, on assumptions made by management. These statements are not guarantees of future performance and involve risks and uncertainties that are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in such forward-looking statements due to numerous factors, including the following: the ability to manufacture and deliver the systems referenced in this release, changes in demand for the Company's products, product mix, the timing of deliveries under the award discussed above, the impact of competitive products and pricing, constraints on supplies of critical components, excess or shortage of production capacity, the ability of the Company to manufacture and ship products in the time period required, actual purchases under agreements, the Company's continuing compliance with U.S. export control laws and regulations, the timely receipt of export licenses for international shipments, the continuing eligibility of the Company to act as a federal contractor, and other risks discussed from time to time in the Company's Securities and Exchange Commission filings and reports. In addition, such statements could be affected by general industry and market conditions and growth rates, and general domestic and international economic conditions. Such forward-looking statements speak only as of the date on which they are made and the Company does not undertake any obligation to update any forward-looking statement to reflect events or circumstances after the date of this release, or for changes made to this document by wire services or Internet service providers.