2007-09-12

ICx Unveils the Next Generation of Ruggedized Fixed Thermal Imagers

The newest VisionIR™ combines high end thermal electronics with streamlined housing and advanced, ruggedized features.

ICx Technologies, a developer of advanced technology solutions for homeland and military security, unveils the next generation of ruggedized thermal imagers at this week’s ASIS International in Las Vegas, NV. With advanced capabilities to protect against water and particulate intrusion, the VisionIR offers a low cost, low power consumption alternative in a fixed thermal unit for the military and commercial security market. The VisionIR is developed and manufactured by ICx Imaging Systems, a business unit of ICx Technologies based in Florida.

Fully customizable and featuring several lens and detector options, the VisionIR offers remote focusing capabilities or can be provided in a focus free alternative. The camera is highly compatible with video analytic applications and provides a new 16mm lens option for an expanded field of view, ideal for surveillance.

"Our next generation VisionIR is specifically designed to protect against seawater, snow, heavy rain and sand intrusion," said Nirav Pandya, General Manager of ICx Imaging Systems. "The on-board Pelco D Protocol, which provides low power consumption as well as easy installation, makes the VisionIR an ideal solution for port, airport, border and commercial surveillance applications."

The VisionIR is environmentally sealed in a nitrogen purged housing which meets NEMA 4X and IP66 specifications. Certified and tested by an independent lab, the VisionIR offers consistent and outstanding performance amid a myriad of adverse weather and daylight conditions.

Specifications

  • Low Power Consumption < 7 Watts
  • Next Generation Thermal Electronics
  • Nitrogen Purged Housing
  • NEMA 4X and IP66 Certified
  • Electronic and Focus Free Lens Options
  • Multi-Protocol
  • Third Party Pan and Tilt Ready
  • IP Addressable

The next generation VisionIR is being demonstrated September 24-27 in booth 1413 during ASIS International at the Las Vegas Convention Center. All ICx Imaging Systems production facilities are ISO 9001:2000 certified. We firmly support an international set of standards for quality and continuous improvement.

About FLIR Systems

FLIR Systems, Inc. is a world leader in the design, manufacture, and marketing of sensor systems that enhance perception and awareness. The Company’s advanced thermal imaging and threat detection systems are used for a wide variety of imaging, thermography, and security applications, including airborne and ground-based surveillance, condition monitoring, research and development, manufacturing process control, search and rescue, drug interdiction, navigation, transportation safety, border and maritime patrol, environmental monitoring, and chemical, biological, radiological, nuclear, and explosives (CBRNE) detection. Visit the Company's web site at www.FLIR.com.

The statements in this release by Earl R. Lewis, and the other statements in this release about the award described above, are forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995. Such statements are based on current expectations, estimates and projections about the Company's business based, in part, on assumptions made by management. These statements are not guarantees of future performance and involve risks and uncertainties that are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in such forward-looking statements due to numerous factors, including the following: the ability to manufacture and deliver the systems referenced in this release, changes in demand for the Company's products, product mix, the timing of deliveries under the award discussed above, the impact of competitive products and pricing, constraints on supplies of critical components, excess or shortage of production capacity, the ability of the Company to manufacture and ship products in the time period required, actual purchases under agreements, the Company's continuing compliance with U.S. export control laws and regulations, the timely receipt of export licenses for international shipments, the continuing eligibility of the Company to act as a federal contractor, and other risks discussed from time to time in the Company's Securities and Exchange Commission filings and reports. In addition, such statements could be affected by general industry and market conditions and growth rates, and general domestic and international economic conditions. Such forward-looking statements speak only as of the date on which they are made and the Company does not undertake any obligation to update any forward-looking statement to reflect events or circumstances after the date of this release, or for changes made to this document by wire services or Internet service providers.

All trademarks, registered trademarks and service marks are the property of their respective owners.

Media Contacts

Angel Bennett
FLIR, Systems, Inc.
2800 Crystal Drive, Suite 330
Arlington, VA 22202
angel.bennett@flir.com