2007-07-19

ICx Technologies Launches New Field-Portable Mass Spectrometer System

First field-portable system supporting liquid and direct air sampling to detect volatile and semi-volatile chemical targets on site

ICx Technologies, a provider of advanced technology solutions for homeland and military security, has unveiled its revolutionary field-portable mass spectrometer system. The system, developed by the ICx Griffin business unit, is comprised of the Griffin 450™ Gas Chromatograph/Mass Spectrometer (GC/MS/MS), multiple sample introduction methods including the handheld Griffin X-Sorber™, and enhanced supporting software.

"We’re proud to launch the first fieldable system that provides lab quality answers with the flexibility to analyze both air and liquid phase samples," said Dennis Barket, CEO of ICx Griffin. "The X-Sorber extends the range of high quality sample collection with a handheld unit that seamlessly docks to the Griffin 450 GC/MS/MS."

The Griffin 450, specialized for transportable and mobile applications, provides laboratory quality chemical analysis in the field for a broad range of compounds, including explosives, chemical warfare agents (CWAs), industrial chemicals, and organic compounds (both volatile and semi-volatile). The Griffin 450 is also equipped with several field-selectable inlet options to accommodate a variety of liquid and gas sample introduction methods, including the Griffin X-Sorber, the world’s first handheld, smart sampler.

Weighing only 3 lbs, the Griffin X-Sorber provides a safe and efficient method for downrange air sampling, eliminating the need to carry heavier instrumentation into a "hot zone."

Designed to operate seamlessly with the Griffin 450 for sample desorption and data download, the X-Sorber provides a handheld option for a broad range of applications, is easy to use and requires minimal training.

The Griffin 450, in tandem with the Griffin X-Sorber, allows for expanded operations as well as on-site detection and analysis. Its unmatched flexibility and mobility make the system ideal for military, emergency response, homeland security and environmental monitoring applications.

Also, the sample archiving capability bodes great potential for the capture of forensic evidence, among other uses.

ICx Griffin has also released its System Software Version 3.0 (GSS 3.0) which provides additional features that allow users to intuitively control the Griffin line of mass spectrometers, including the new Griffin 450 system. GSS 3.0 offers an interface that changes based on three different user levels (operator, developer or administrator). Additional software features include tools for more in-depth data analysis, qualification and quantification as well as enhanced real-time identification capabilities.

ICx Griffin is the first company to provide field-portable mass spectrometer systems capable of providing more comprehensive and accurate information through multidimensional mass analysis (MS/MS). ICx Griffin products provide accurate information for making critical decisions regarding life, safety, and the environment.

About FLIR Systems

FLIR Systems, Inc. is a world leader in the design, manufacture, and marketing of sensor systems that enhance perception and awareness. The Company’s advanced thermal imaging and threat detection systems are used for a wide variety of imaging, thermography, and security applications, including airborne and ground-based surveillance, condition monitoring, research and development, manufacturing process control, search and rescue, drug interdiction, navigation, transportation safety, border and maritime patrol, environmental monitoring, and chemical, biological, radiological, nuclear, and explosives (CBRNE) detection. Visit the Company's web site at www.FLIR.com.

The statements in this release by Earl R. Lewis, and the other statements in this release about the award described above, are forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995. Such statements are based on current expectations, estimates and projections about the Company's business based, in part, on assumptions made by management. These statements are not guarantees of future performance and involve risks and uncertainties that are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in such forward-looking statements due to numerous factors, including the following: the ability to manufacture and deliver the systems referenced in this release, changes in demand for the Company's products, product mix, the timing of deliveries under the award discussed above, the impact of competitive products and pricing, constraints on supplies of critical components, excess or shortage of production capacity, the ability of the Company to manufacture and ship products in the time period required, actual purchases under agreements, the Company's continuing compliance with U.S. export control laws and regulations, the timely receipt of export licenses for international shipments, the continuing eligibility of the Company to act as a federal contractor, and other risks discussed from time to time in the Company's Securities and Exchange Commission filings and reports. In addition, such statements could be affected by general industry and market conditions and growth rates, and general domestic and international economic conditions. Such forward-looking statements speak only as of the date on which they are made and the Company does not undertake any obligation to update any forward-looking statement to reflect events or circumstances after the date of this release, or for changes made to this document by wire services or Internet service providers.

All trademarks, registered trademarks and service marks are the property of their respective owners.

Media Contacts

Angel Bennett
FLIR, Systems, Inc.

2800 Crystal Drive, Suite 330
Arlington, VA 22202
angel.bennett@flir.com