2007-03-19

ICx Technologies Unveils a New Deterrence Camera with Non-Lethal Incapacitating Capabilities

The Illuminator™ combines a low-light CCD camera with a high-power spotlight to detect and immobilize intruders.

ICx Digital Infrared Imaging, a business unit of ICx Technologies, a national leader in the development of advanced technologies for effective security solutions, now offers the military and commercial security market an affordable deterrence system that utilizes a low-light CCD camera with a high-power spotlight to detect, deter, and immobilize intruders.

The Illuminator’s spotlight, available in both a 7.5 and 12 million-candlepower (MCP) option, can temporarily disorient encroaching individuals who are within a one-mile radius when used in its deterrence mode. Additionally, it can be outfitted for covert near-IR capability.

"The camera is unique because it can Illuminate targets and show security forces where intrusion is occurring, making it very useful for first responders," said Nirav Pandya, General Manager of ICx Digital Infrared Imaging. "It has also been designed for ease of integration with legacy or new equipment," Pandya said. "For instance, it can be combined with industry-leading ICx millimeter wave radars to create a highly effective and multi-functional surveillance system that can visibly illuminate and track objects automatically."

The advantages of this camera are many, but it can be offered at a relatively low cost as compared to other covert cameras in the marketplace. Additionally, it can be used as a powerful tool to complement existing CCTV systems that need remote deterrence capability. Furthermore, it can be used effectively for search and rescue and crowd control.

Specifications

  • The 7.5 MCP spotlight can Illuminate targets up to 1 mile
  • The 12 MCP spotlight can illuminate targets up to 1.5 miles
  • An optional filter is available for covert near-IR operation
  • An optional CCD lens doubler is available for increased CCD range performance
  • For standalone capability, the camera can be controlled through a graphical user interface (GUI) or through a low-cost joystick
  • Optional auto-tracking via integrated ground based radar system
  • Can be deployed for remote operation by use of ICx Mobile Platforms
  • Continuous 360-degree pan capability
  • Optional thermal camera provides convert viewing of target while spotlight allows for visualization & interception by ground forces, response teams, or search & rescue.

ICx Digital Infrared Imaging is known as a leader in the custom development, design and manufacture of thermal imaging systems. It will debut the Illuminator to ISC West Expo in booth 32003 in Las Vegas from March 28-30.

About FLIR Systems

FLIR Systems, Inc. is a world leader in the design, manufacture, and marketing of sensor systems that enhance perception and awareness. The Company’s advanced thermal imaging and threat detection systems are used for a wide variety of imaging, thermography, and security applications, including airborne and ground-based surveillance, condition monitoring, research and development, manufacturing process control, search and rescue, drug interdiction, navigation, transportation safety, border and maritime patrol, environmental monitoring, and chemical, biological, radiological, nuclear, and explosives (CBRNE) detection. Visit the Company's web site at www.FLIR.com.

The statements in this release by Earl R. Lewis, and the other statements in this release about the award described above, are forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995. Such statements are based on current expectations, estimates and projections about the Company's business based, in part, on assumptions made by management. These statements are not guarantees of future performance and involve risks and uncertainties that are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed or forecasted in such forward-looking statements due to numerous factors, including the following: the ability to manufacture and deliver the systems referenced in this release, changes in demand for the Company's products, product mix, the timing of deliveries under the award discussed above, the impact of competitive products and pricing, constraints on supplies of critical components, excess or shortage of production capacity, the ability of the Company to manufacture and ship products in the time period required, actual purchases under agreements, the Company's continuing compliance with U.S. export control laws and regulations, the timely receipt of export licenses for international shipments, the continuing eligibility of the Company to act as a federal contractor, and other risks discussed from time to time in the Company's Securities and Exchange Commission filings and reports. In addition, such statements could be affected by general industry and market conditions and growth rates, and general domestic and international economic conditions. Such forward-looking statements speak only as of the date on which they are made and the Company does not undertake any obligation to update any forward-looking statement to reflect events or circumstances after the date of this release, or for changes made to this document by wire services or Internet service providers.

All trademarks, registered trademarks and service marks are the property of their respective owners.

Media Contacts

Angel Bennett
FLIR, Systems, Inc.

2800 Crystal Drive, Suite 330
Arlington, VA 22202
angel.bennett@flir.com