Radar Enabling Software
Distributed Radar and Sensor Network Control

Forewarned is Forearmed.

Working with an array of standard ground based radars, the STS Control Station graphically presents detected intruders on a computer screen and sounds an alarm. Using the intruder’s location received from the radar, the STS Control Station can automatically point a camera to identify the threat. Now, response can be appropriate and efficient as the intruder is tracked real time.

Whether part of a portable, mobile or fixed radar installation, the STS Control Station can simultaneously monitor multiple radars and cameras. And when needed, several STS Control Stations in dispersed sites can be networked as part of one wide area surveillance network. One installation contains more than 50 radars.

With a rich set of reporting, interfacing, administrative and user controls, the STS Control Station is an intuitive and easy to operate mini-annunciator for force protection and high value site security applications.

The STS Control Station may be used in conjunction with the STS-350, STS-12000 and MDAS.